This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SimpleBLEPeripheral WITH serial interface (UART) Sleep mode

Other Parts Discussed in Thread: CC2540, CC2640

Hello ..

I am running SimpleBLEPeripheral code  WITH serial interface (UART) from another controller . I have full control sending  advertizing data from remote uController  at the rate that I need  ( 5s and 1min)..  and cc2540 does advertise accordingly 

The problem I have is i never  see cc2540  go to sleep in between adv.   I have enabled POWER_SAVING compiler option .. but I do not see it ever execute after all tasks complete. 

My intention is to put cc2540 to sleep after each advertizing and have remote (via UART ) communication wake it up so that it can advertise again  as commanded by remote uC.

Any suggestion please help . I am running on BATT and need to save power .

Many thanks

Alex