Other Parts Discussed in Thread: CC2650, Z-STACK
Hello All,
I am trying to learn Zigbee HA applications with the help of CC2650.
I would like to communicate between two CC2650(One as End device other one as Coordinator(ZNP+Ztool))
With the help of Zstack documents and some answers from this forum I am able to set up below test environment.
1. Sample Switch (CC2650 End Device) :
I have flashed "Sample Switch" application in this device in LCD screen able to see below lines
"Up : ToggleLight"
"Rt : EZ-Mode"
"Select: Main"
2. Sample Light (Ztool+ZNP) :
- I have flashed "znp_coordinator_pro.hex"
- In Ztool script window executed "znp-bringup.zjs" with proper COM port changes.
- in Ztool, I have given ZB_PERMIT_JOINING_REQUEST with time-out value as 0xFF(Allow always for joining)
- in Ztool , I have given UTIL_GET_DEVICE_INFO and the response was
<TX>07:30:03.86 COM35 UTIL_GET_DEVICE_INFO (0x2700)
<RX>07:30:03.88 COM35 UTIL_GET_DEVICE_INFO_RESPONSE (0x6700)
Status: SUCCESS (0x0)
IEEEAddr: 0x00124B0007BAC004
ShortAddress: 0x0000
DeviceType: COORDINATOR (0x1)
DeviceState: DEV_ZB_COORD (0x9)
NumAssocDevices: 0x00
AssocDevicesList
Could I assume that Zigbee Coordinator is successfully started?
Then, I have pressed SW2 in sample switch(CC2650) and it is trying in EzMode to join any of the available network(??)
Below is the Packet Sniffer capture
Can anyone help me to make communication between end device and Coordinator?