Other Parts Discussed in Thread: CC2650, CC2640, BLE-STACK
Hi,
During OAD I recieve message:
"Wrong image type !"
"Image that was selected was of type: B, which is the same as on the periperhal...."
Actions I took
1. Using SDK 2.1
2. My Project is branching out from SensorTag project.
3. Enabled FEATURE_OAD.
4. Downloaded hex file image via debugger to CC2650.
5. using options > Output Converter: Created another .bin file for download (gave this image a differnet internal sw version so I can check that download succeded)
6. tried downloading this image via SensorTag App
7. recieved the message above.
Questions
Do I have to specify the BANK somewhere prior to bin conversion?.
Have I missed something?.
Thanks in advance
Tamir