Other Parts Discussed in Thread: CC2640
Hi,
I came across a problem with the SPPBLEServer I am using to bridge between the CC2640 serial port and an iPhone running a BLE application.
This exhibits as the serial -> BLE blocking when I try to send "too much" data through (e.g. a couple of hundred characters).
I've tracked this down to SPPBLEServer.c, SPPBLEServer_taskFxn(), SBP_UART_DATA_EVT
What happens is that the sending of the notification with SerialPortService_SetParameter() fails.
Rather than retry the code stops, which has the effect that the failed message remains queued up until more serial Rx data is received, at which time the messages are correctly transmitted from the queue to the BLE device
A fix that works for me is
//Send the notification
retVal = SerialPortService_SetParameter(SERIALPORTSERVICE_CHAR_DATA, pMsg->length, pMsg->data);
if(retVal != SUCCESS)
{
LCD_WRITE_STRING_VALUE("NotiFAIL:", retVal, 10, LCD_PAGE4);
LCD_WRITE_STRING_VALUE("Data length:", pMsg->length, 10, LCD_PAGE5);
LCD_WRITE_STRING(pMsg->data, LCD_PAGE6);
// AJL - Don't block on notification send failure...
if(!Queue_empty(appUARTMsgQueue))
{
// Wake up the application to flush out any remaining UART data in the queue.
Semaphore_post(sem);
}
}