Is there a way to detect when a peripheral device disconnects ??
I want to implement a backup time where the peripheral device can self disconnect after xx minutes even if the central device did not
I see there is a event when the device connection but I do not see an event when the peripheral is disconnected
Is there a what to query the current connection status ???
or Is there an event call back when the peripheral gets disconnected ??
Thanks
Brian