Hello,
I am using CC2540 USB BLE Dongle with PC Application implemented in .Net.
Following Bond parameter has been set during initialization of this dongle.
GAPBOND_PAIRING_MODE -> 01-GAPBOND_PAIRING_WAIT_FOR_REQ
GAPBOND_MITM_PROTECTION -> 00-Disabled
GAPBOND_BONDING_ENABLED -> 01-Enabled
GAPBOND_IO_CAPABILITIES -> 03-No I/p No O/p
We are facing some issues in bonding with the central devices, and receiving terminate command with reason code 05.
When we flash the host test image with bonding enabled, the issues is not occurring till some 10+ central devices.
After that we start receiving termination command with 05, once the connection gets established.
So, We are trying to erase the bonding be setting the following Bond parameter.
GAPBOND_ERASE_ALLBONDS -> 00-No Value
But the execution of the above Bond set parameter give Parameter out of range as resultant. Please find the below code.
--------------------------------------------------------------------
[23] : <Tx> - 06:19:17.741
-Type : 0x01 (Command)
-OpCode : 0xFE36 (GAP_BondSetParam)
-Data Length : 0x04 (4) byte(s)
ParamID : 0x0409 (1033) (GAPBOND_ERASE_ALLBONDS)
ParamLength : 0x01 (1)
Value : 00
Dump(Tx):
0000:01 36 FE 04 09 04 01 00 .6......
--------------------------------------------------------------------
[24] : <Rx> - 06:19:17.759
-Type : 0x04 (Event)
-EventCode : 0x00FF (Event)
-Data Length : 0x06 (6) bytes(s)
Event : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
Status : 0x18 (24) (A Parameter Is Out Of Range)
OpCode : 0xFE36 (GAP_BondSetParam)
DataLength : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 18 36 FE 00 ......6..
--------------------------------------------------------------------
Can some one suggest me the usage of Bond set param of Erase All Bonding with correct value.
Thanks in Advance.
Regards,
Ramesh Kumar