This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SimpleBLEPeripheral - P0_0 P1_2 Pins

Other Parts Discussed in Thread: CC2650, CC2541

Hi,

I'm using simpleBLEPeripheral example project and I'm having problems with the configuration of some pins. In main function i can control all of them without problems before than osal_start_system is called. Then pins P0_0 and P1_2 are set HIGH somewhere. I can't find the snippet where it occurs since i don't want this. 

How can I do it? Where does this pins are setted HIGH? 

thanks,
Marco