Other Parts Discussed in Thread: CC2650
Tool/software: TI-RTOS
I'm working on a CC2640 4x4 custom board, ble_sdk_2_02_01_18, CCS 6.2, XDS 200 debugger,
BTool v1.41.16, simple_peripheral_lp_app.
The custom board has two SPI slaves, one for the external flash and another for sensor measurements.
I am running a clean copy of simple_peripheral through the custom board. I am looking at both the SPI
chip select signals on the scope.
BTool is showing the OAD blocks being transmitted, though the OAD with clean simple_peripheral always
ends in a CRC error.
The scope shows the external flash chip select always asserted low. The other SPI slave chip select is
mostly high but also becomes asserted during OAD. Is there a way to prevent this? Code snippets are
appreciated.
Thanks,
Priya