This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1350: Nothing happens when running SPP BLE server example

Part Number: CC1350
Other Parts Discussed in Thread: CC2650, BLE-STACK, LAUNCHXL-CC2650

Tool/software: Code Composer Studio

I'm trying to run the SPP BLE server example on an CC1350 LaunchPad, but after I build and download the stack and app projects nothing happens after downloading the app project. All run, paus, step, etc button is greyed out and the debugger dont run to main. Does anyone know for what reasons this  might be happening?

/Michael

  • Hello Michael,

    You cannot run CC2650 projects on the CC1350. The BLE-Stack v2.2.1 includes sample applications under the \examples\cc1350lp folder of the SDK which are compatible with the CC1350. We do not have a CC1350 version of SPP BLE but you can try taking the CC1350LP simple_peripheral sample application and porting the application files to this project. Otherwise, it's recommended to use a CC2650 LaunchPad (LAUNCHXL-CC2650) for this project as it is BLE-only.

    Best wishes