This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640: Unknown Reset when put scope probes on the output of PA

Part Number: CC2640

Tool/software: TI-RTOS

I use 8 GPIOs of cc2640 to generate a AC signal,
and convert it to higher voltage signal by OP and PA.
When I put the scope probes on the output of PA(There is no load on PA output),
cc2640 will reset but I don't know why.
The Output Signal:
- ACV is about ±350~400V
- Frequency is about 100Hz.
FW: Based on SimpleBLEPeripheral(TI_RTOS:2.13.00.06)
MCU: cc2640
Why cc2640 reset? How to find the root cause and fix it?