Other Parts Discussed in Thread: BLE-STACK, , CC2540
Hello.
I have a CC2640 module flashed with HostTestCC2650EM_app BLE-STACK V2.2.1.
I sent over UART next commands to initialize the device as peripheral:
1. GAP DEVICE INITIALIZATION
2. GAP CONFIGURE DEVICE ADDRESS
3. GAP UPDATE ADVERTISING DATA
4. GAP MAKE DISCOVERABLE
Next step, I tried to connect it with a CC2540 dongle (as central).
In BTool I can see that CC2640 module is discovered. When I try to connect I receive GAP_EstablishedLink event, but then the connection is terminated immediately (I receive in BTool GAP_TerminateLink event with reason "Failed To Establish").
With TI Packet Sniffer, I can see that slave is not responding to any connection event (see attachment below).
What can be done for the connection to be stable? Is any other command to be sent to CC2640 to respond on this events?