Hello,
SmartRF Studio 7 seems to allow me to configure the following parameters for a custom target
IO Configuration, Device, Package, Front-end and Output Power
What about some of the other parameters like CAP ARRAY delta configuration, LF Clock Source and such ? We tried to load some code on the CC26xx to disable the internal CAP ARRAY but that doesn't seem to take effect ? Is the configuration loaded on to CC26xx via the application load, used when running continuous tx/ rx tests with SmartRF Studio 7 ? Is there a register view for SmartRF Studio7 for CC26xx so I can verify all the configuration registers ?
Also, my customer has observed that the RF output of the same board with same firmware load is different with different versions of the SmartRF Studio 7 ? The specific versions he is using are version 2.2.0 and 2.6.0 - why might that be ?
Thanks,
Padmaja