This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2650: CODE OR HEX FILE CAN NOT LOAD TO CC2650

Part Number: CC2650

Tool/software: Code Composer Studio

Sir,

i have custom board designed with cc2650 and a sensor tag DEV pack DEBUGGER.

i try to load one of the hex file provided by Bluetooth stack 2.2  through flash programmer 2.

but the code is not going through it shows .ERROR UPLOADING THE CODE FAILED TO LOAD FROM 0X00000000;

in the edit field FP2 i can read the memory pages MAC address of cc2650 but code is not going through

why...??????

please do  solve this problem soon.

because no one is replaying correctly . i want to clear this with zero error