This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2640R2: External Flash memory

Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: SYSBIOS

Tool/software: Code Composer Studio

I have two main question on access external flash memory.

First when i want to reference the ExtFlash file to my program with  #include <ti/mw/extflash/ExtFlash.h> It will always report me error with 

":Description Resource Path Location Type
unresolved symbol ExtFlash_open, first referenced in ./memory.obj memory_ccs C/C++ Problem"

But if i do it with  #include <ti/mw/extflash/ExtFlash.c>. It doesn't have these kind of problem anymore, but i know it is not a suitable method.

Then i tried to test the ExtFlash_open() function, i made a very simple coding:

Board_initGeneral();

SPI_Handle spi;
SPI_Params spiParams;

SPI_init(); // Initialize the SPI driver
SPI_Params_init(&spiParams); // Initialize SPI parameters
spiParams.dataSize = 8; // 8-bit data size
spi = SPI_open(Board_SPI0, &spiParams);
if (spi != NULL) {
System_printf("SPi transfer is open");
}

bool isOpen = ExtFlash_open();
if (isOpen == false){
System_printf("No external flash memory");
}
else{
System_printf(" external flash memory open wake up");
}
return(0);

I have already checked the support device list in ExtFlash.c, i saw the device type

{
.manfId = MF_MACRONIX, // Macronics
.devId = 0x14, // MX25R8035F
.deviceSize = 0x100000 // 1 MByte (8 Mbit)
},

The result is that is SPI can always start, but the return value of the ExtFlash_open() is always false. Does anyone know any possible solution for that?