Other Parts Discussed in Thread: CC2640
Hi,
we are using the SPP_Server_OAD_onChip project with our designed CC2640R2F_5XD board. SDK version 1.35.0.33
teh board was fixed with 29 bytes of advertisement data, advertising interval of 100ms, TX power 5 dBm, advertising at 3 channels.
cryztal was ON for 5 ms. we enabled POWER_SAVING in predefined symbol.
CR2032 battery was used here.
the battery was drained from 100% to 70% in 3 days and stopped
Peripheral(SPP_server) was not connected to central(SPP_client) during this time. Board was only on 100 % advertisement state during this 3 days.
but the TI calculator shows 41 days of life with above configuration parameters.
Please suggest a solution to solve our mistake to achieve the 40 days life.
thanks,
narayanan