This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650 custom board HAL_SYSTEM_RESET() issue

Other Parts Discussed in Thread: CC2650

Hello, friends.

We have got a custom board based on CC2650RHB chips and we are testing OAD protocol at the moment.

Sometimes (very seldom) CC2650 doesn't restart with HAL_SYSTEM_RESET() command. It helps only hardware reset or switch off power supply.

Our invironment and configuration is:

VDDS=VDDR= 1.8V External LDO mode (DC/DC is off)

IAR 7.70

BLE stack 2.2.1

When this issue happens we haven't any osscillation on LF and HF resonators that is why I think this isn't a halt...

We are using KX-327FT by Geyer manufacture with 12 pF load capacitors, maybe it's problem and we need to use load capacitors with more values of capcity, but I am not sure that It't thereason of issue...