Other Parts Discussed in Thread: CC1020, CC1100
I am using the CC1020 ICs in an AX.25 protocol based environment. My problem is that only one byte i.e. 0x7E is recognised as sync word in AX.25, whreas including 2 bytes preamble and 2 bytes Sync word a total of 4 bytes are required for CC1020. How can i configure it to use only 0x7E instead of these 4 bytes as Sync word?