Hi,
I have a trouble with analog FM demodulation, could somebody help me with these:
1) what are the exact requirements to read data from SOFT_RX_DATA_OUT and enable related trigger clock on GPIO (=CLKEN_SOFT).
Under which condition the CLKEN_SOFT and SOFT_RX_DATA_OUT are available? There will be great any map/diagram/etc. that can clear this.
I run some tests and it seems that clock and data are only available in transparent mode, and I can get minimum clock at about 31kHz (at minimal RX filter BW).
2) What are exact meaning of SOFT_RX_DATA_OUT as user's guide talks about instantaneous frequency offset (in par. 4.1.4) and register description states:
soft-decision symbol data in normal/transparent receiver (p. 100).
Thank you
Martin