I have a CC2540 mini dev kit. I have flashed the dongle with firmware file CC2540_USBdongle_HostTestRelease_All.hex using the CC Debugger which has a green light. After flashing the dongle displays a red LED. When I try to associate the usb_cdc_driver_cc2540.inf USB driver though, Windows XP (SP3) reports "Device cannot start (code 10)". I've read posts about this in this forum but cannot find a solution and I've been trying for days.
Also if after flashing using action Erase, program and verify, which reports success, if I then execute action "Verify against hex file" I get an error "CC2540 - ID7369: Error in HEX file verification".
Hope someone can help
Martin