There are two pins to connect to a 24MHz crystal oscillator, but I want to use a VCTCXO with a single clock output for the CC2630 clock input. Can I connect this to one of the two crystal pins (X24M_N or X24M_P)?
If I can drive the XTAL input with an oscillator, then what are the specs on the interface?
For example, see section 4.11.3.4 on this datasheet: http://www.ti.com/product/CC3200/datasheet/specifications
Thanks,
Ben