Other Parts Discussed in Thread: CC1120
Hi,
We are doing a design using CC1120 + MSP430 and the DC2DC TPS62730
Could you advise what value of a input buffer capacitor (Cbuf) I should use with the TPS62730 assuming that we only transmit for a duration of 1 millisecond every 1 second with 4dBm out put power.
Or in short - about 27mA current consumption for duration of 1 ms tx bursts...
We are using a coin cell battery(CR2032).
What should be the capacitance of the Cbuf?
Attached is the deisgn of the DC2DC block
Thank you,
Yaniv