I have a customer using the CC2530 and is failing FCC in Rx mode around the 2nd harmonic 2.4GHz. They were able to improve the performance by a couple of dB by adding a 5.6pF cap in parallel with the pull-down resistor (56K ohm) on Rbias pin #30. They are not sure if this is a valid fix since they do not know what the functionality of Rbias pin is and if a cap will cause problems. Can you comment?