Other Parts Discussed in Thread: CC2530, Z-STACK
Hi everyone,
I was wondering if there is a way to verify that the frequency agility feature of the Zigbee Pro specification is functioning in the Z-stack. I am using a CC2530 flashed with the CC2530ZNP-Pro.hex file provided in the ZAP-MSP430-1.0.0 collection of files. I am running a network with a singe coordinator and 5 end devices. The end devices are configured to send data every 0.5 seconds to the coordinator. All the devices on the network have a full channel list.
Is there a ZNP command I can send to verify that frequency agility is turned on?
If there is no ZNP Command to verify frequency agility, how could I force the Zigbee network to change channels using it's frequency agility feature?
Thanks in advance.