This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No WIFI Icon/WPA_GUI on AM335x



Hi,

I have been trying to configure the wifi on AM335x-EVM-sk for a while.

I have tried():
root@am335x-evm:~# ifconfig wlan0 up                                            
                                                                                
ifconfig: SIOCGIFFLAGS: No such device

and I also tried this:
root@am335x-evm:/usr/sbin# wpa_supplicant -d -Dnl80211 -c/etc/wpa_supplicant.con
                                                                                
f -iwlan0 -B                                                                    
                                                                                
wpa_supplicant v2.1-devel                                                       
                                                                                
random: Trying to read entropy from /dev/random                                 
                                                                                
Successfully initialized wpa_supplicant                                         
                                                                                
Initializing interface 'wlan0' conf '/etc/wpa_supplicant.conf' driver 'nl80211'
ctrl_interface 'N/A' bridge 'N/A'                                               
                                                                                
Configuration file '/etc/wpa_supplicant.conf' -> '/etc/wpa_supplicant.conf'     
                                                                                
Reading configuration file '/etc/wpa_supplicant.conf'                           
                                                                                
update_config=1                                                                 
                                                                                
ctrl_interface='/var/run/wpa_supplicant'                                        
                                                                                
eapol_version=1                                                                 
                                                                                
ap_scan=1                                                                       
                                                                                
fast_reauth=1                                                                   
                                                                                
device_name='Blaze'                                                             
                                                                                
manufacturer='TI'                                                               
                                                                                
model_name='Wilink'                                                             
                                                                                
model_number='wl18xx'                                                           
                                                                                
serial_number='12345'                                                           
                                                                                
driver_param='use_multi_chan_concurrent=1 use_p2p_group_interface=1'            
                                                                                
p2p_go_max_inactivity=60                                                        
                                                                                
p2p_go_ht40=1                                                                   
                                                                                
disassoc_low_ack=1                                                              
                                                                                
concurrent[  772.160866] cfg80211: Calling CRDA to update world regulatory domai
n                                                                               
                                                                                
_sched_scan=1                                                                   
                                                                                
p2p_disabled=1                                                                  
                                                                                
Could not read interface wlan0 flags: No such device                            
                                                                                
nl80211: Driver does not support authentication/association or connect commands
                                                                                
nl80211: Remove monitor interface: refcount=0                                   
                                                                                
netlink: Operstate: linkmode=0, operstate=6                                     
                                                                                
[  772.324086] cfg80211: World regulatory domain updated:                       
                                                                                
[  772.329403] cfg80211:  DFS Master region: unset                              
                                                                                
[  772.333795] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gai
n, max_eirp), (dfs_cac_time)                                                    
                                                                                
[  772.343612] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 20
00 mBm), (N/A)                                                                  
                                                                                
[  772.352024] cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 20
00 mBm), (N/A)                                                                  
                                                                                
[  772.360440] cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 20
00 mBm), (N/A)                                                                  
                                                                                
[  772.368855] cfg80211:   (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 20
00 mBm), (N/A)                                                                  
                                                                                
[  772.377259] cfg80211:   (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 20
00 mBm), (N/A)                                                                  
                                                                                
Could not read interface wlan0 flags: No such device                            
                                                                                
nl80211: Set mode ifindex 0 iftype 2 (STATION)                                  
                                                                                
nl80211: Failed to set interface 0 to mode 2: -19 (No such device)              
                                                                                
wlan0: Failed to initialize driver interface                                    
                                                                                
Failed to add interface wlan0                                                   
                                                                                
wlan0: Cancelling scan request                                                  
                                                                                
wlan0: P2P: Station mode scan operation not pending anymore (sta_scan_pending=0
p2p_cb_on_scan_complete=0)                                                      
                                                                                
wlan0: Cancelling authentication timeout                                        
                                                                                
wlan0: cancel_sched_scan called when no sched scan

Any suggestions?