Other Parts Discussed in Thread: WL1837MOD
I am working on a solution for streaming audio over Wi-Fi. I'm evaluating the WL1837MOD and the AM335x processors based on TI's Streaming Audio Reference Design.
I have three AM335x EVM boards and am using GStreamer. I am using the latest SDK - version 1.00.00.03.
The problem is that I'm getting glitches/dropouts in the streaming audio while listening via the on board headphone output.
I was directed to this forum from the guys over in the Sitara Processors Forum. I initially posted there as I was having some issues just over ethernet, however with some pipeline optimization and buffering, it is now working smoothly over ethernet.
I am using one EVM as the server, creating a Wi-Fi network using hostapd - there is no router involved. I'm using the best channel I can find at 5GHz. I am using another EVM as the client (and have tried a third EVM as a client to make sure it wasn't just this particular device). Using iperf, I can get up to 100Mbps over the Wi-Fi link sending UDP packets.
There are four scenarios where it is working fine:
- Stream from server EVM to client EVM over ethernet, playing back via on board headphone output.
- Stream from server EVM to laptop over Wi-Fi.
- Stream from server EVM to client EVM over Wi-Fi, saving the data to a .wav file on the local RAM disk, transferring it to my laptop, and playing it back there.
- Stream from server EVM to server EVM over localhost, playing back via on board headphone output (only uses ~50% CPU, so not over doing it)
I am streaming a 96k, 24 bit, 2 channel flac file. I have resampled it down to 8k, and the problem persists. So I'm wondering if it is a bus contention issue or some other type of issue when using Wi-Fi and the EVM's on board audio codec (connected via I2S and the McASP) simultaneously.
Gstreamer does not indicate any buffering or packet loss/order problems when this occurs (it did before I got the buffering set up etc).
Even if I set the buffer to 5 seconds it behaves the same.
My pipelines are as follows:
Server:
gst-launch-1.0 -v filesrc location=/run/dsb.flac ! flacparse ! flacdec ! audioconvert ! rtpL24pay ! udpsink host=10.192.0.100 port=5000
Client (streaming to on board audio codec):
gst-launch-1.0 -v --gst-debug=udpsrc:5 --gst-debug=rtpL24depay:4 --gst-debug=rtpjitterbuffer:4 udpsrc port=5000 caps="application/x-rtp, media=(string)audio, clock-rate=(int)96000, encoding-name=(string)L24, encoding-params=(string)2, channels=(int)2, payload=(int)96" ! rtpjitterbuffer mode=2 latency=1000 ! rtpL24depay ! audioconvert ! alsasink
Client (streaming to .wav on RAM disk):
gst-launch-1.0 -v --gst-debug=udpsrc:5 --gst-debug=rtpL24depay:4 --gst-debug=rtpjitterbuffer:4 udpsrc port=5000 caps="application/x-rtp, media=(string)audio, clock-rate=(int)96000, encoding-name=(string)L24, encoding-params=(string)2, channels=(int)2, payload=(int)96" ! rtpjitterbuffer mode=2 latency=1000 ! rtpL24depay ! audioconvert ! wavenc ! filesink location=/run/out.wav
Any suggestions?
Andrew