Hello,
I use omap3evm board from Mistral with Wireless Connectivity Card which incorporates a WL1271 chip (required bluetooth firmware version is TIInit_7.2.31.bts).
I can hear sound in my headset only if I send sound data to WL1271 over PCM. I tried bluez4 config option SCORouting to both HCI and PCM, but it didn't help.
The same situation can be observed in e.g. TI_OMAP35x_WL1271_6.1.0.0.144 demo package (see bluetooth demo script BT_HFP_Play.sh):
bluez4 configures audio on BT chip, but sound data is sent over PCM.
So It looks like BT chip is always expecting audio from PCM regardless how bluez4 is configured.
Is there a way to configure audio routing for wl1271 chip if I want to choose either HCI or PCM ?
Thanks,
Sergey