Hi All,
In my product i have a 84.5K/1% resistor connected between VBAT and my battery. When reading
the values i get from the PM_GET_DATA command, i do see the figures following the voltage change but when i increase the voltage to more then 3.879V, the reading stops following the voltage. On the PPWC, the VBAT monitoring is set to ON with a 84.5K resistor defined. The figures i get are:
"Lowest measurable voltage is in the range of 1.86 to 2.38V"
"Highest measurable voltage is in the range of 3.19 to 4.27V"
So i do not see any reason for it to stop at 3.879V.
Any ideas?
Thank you,
Nir.