This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 Programming

Other Parts Discussed in Thread: CC2540, TPS62730

Hi,

I am new to BLE..I've puechased a seperate CC2540 IC..

How to burn the Program to it??

Do we need to use CC Debugger??

thank you..

  • Assuming that you have a CC2540EM, you will need

    1. SmartRFEB05 or A combination of CC Debugger with SoC BB

    2. SmartRF Flash Programmer SW to flash the CC2540

    if you have your own CC2540 board, follow the CC Debugger guide on how to connect the board directly to the CC Debugger. You will need five pins from your board essentially. VDD, GND, Reset, DD and DC.

  • sry, i don't have the CC2540 evaluation module..

    i have only the IC..

  • You will need to make a board similar to the CC2540 evaluation module to be able to use the chip. The chip on itself cannot be used.

  • Thank you..

    Can i take the reference design given in the TI website for the CC 2540 EM ??

  • Absolutely. We highly recommend that our customers use the reference design and follow it as closely as possible.

  • Hi, 

    We have started building our custom board following the reference design.  I understand from the documents that the debug interface is meant for downloading in to the flash for 8051.  The software also seems to have the flash programmer.  What is the hardware tool that I require -- anything similar to the JTAG programmers normally used with the microcontrollers --  how do I buy it.  Please point me to the right tools.

  • Hi Raghav,

    I recommend the CCdebugger:

    http://www.ti.com/tool/CC-DEBUGGER

    Cheers

  • Hi,

    Is there any alternate way to program the CC2540 IC which we soldered in our custom board  without using the Debugger??

    Also what is the use of Smart RF flash programmer??? Is it available for free?? 

  • Yes, you can also use the SmartRF05EB. It is included in the CC2540DK. 

    SmartRF flash programmer is a PC tool for programming the CC2540 via the CCdebugger or the SmartRF05EB. It is for free.

  • Hi,

    What is the Cross compiler Tools available for CC2540 IC??

    I have Smart RF Flash Programmer and CC Debugger and my own designed Customboard..

    Thank you..

  • Hi Raghav,

    The only supported compiler is the one included in the IAR Embedded Workbench environment.

    Note that you can download images using Over the Air Download (OAD), which is part of the newly released BLEv1.3. This however requires you to initially program a bootloader via ex. CC Debugger.

    Best Regards

  • Hi,

    Thanks..

    However i've IAR free version..Will I  be able to complete the task with the trial version or should I purchase the full version??

  • Hi Raghav,

    Raghav G said:
    Will I  be able to complete the task with the trial version or should I purchase the full version??

    That my friend, depends completely on the solution and your skills/experience with embedded wireless systems. If you have the founding, buy it :) 

    If you could tell me a bit about your idea I might be able to hint an estimate of required work.

    Best Regards

  • Hi,

    Thanks..

    I am trying to build a small security kinda system in my project with CC2540 IC..In my board we just have an IC,Antenna and a Power supply..

    Hence we try to write a code that would sniff the nearby devices and provide authentication system..

  • Well, 

    If you

    • have an intermediate knowledge of c-programming.
    • have read and understood the TI BLE Software developers Guide.
    • have gotten familiar with our BLE Stack API and project examples.
    it should take you a couple of days of putting together the software based on keyfobdemo or simpleBLEperipheral for a decent proof of concept. 
    Best Regards.
  • thanks,

    can you give me the correct working source code for the keyfob or the simple BLE peripheral?

  • Hi Raghav,

    The example projects you are looking for are available in the stack installer, which can be downloaded at www.ti.com/ble-stack.

    Assuming you have installed the stack in the default directory:

    Keyfobdemo is found at C:\Texas Instruments\BLE-CC254x-1.3\Projects\ble\KeyFob\CC2540DB (If you have a CC2540 Keyfob HW)

    SimpleBLEPeripheral is found at C:\Texas Instruments\BLE-CC254x-1.3\Projects\ble\SimpleBLEPeripheral\CC2540DB (If you have a CC2540 EM HW)

    Don't forget to take a look at the documentation found at C:\Texas Instruments\BLE-CC254x-1.3\Documents

    Best Regards

  • thanks..

    Sorry i don't have the stack installed..

    We just have the IC and going to get the Debugger..

    Can you provide the source code in .pdf or .txt formats??

  • Hi Raghav,

    Raghav G said:
    Sorry i don't have the stack installed..

    Install it (it's free) and read the included documentation. 

    Raghav G said:
    Can you provide the source code in .pdf or .txt formats??

    No. That is simply not possible.

    Br

  • Thanks

    I've installed it..

  • Hi,

    The converter TPS 62730 is it essential for the CC2540 IC??

    I am using this IC in my own custom board!!

  • No, the TPS62730 is not essential for the CC2540. The CC2540 can run directly from any power source providing between 2.0 V and 3.6 V.

    The TPS62730 is a 2.1 V buck regulator often used to reduce the power consumption of CC2540. The digital core and radio inside CC2540 is running off an internal 1.8V LDO, so by using a high efficiency external regulator you can reduce the power loss in the LDO (or in other words: increase the efficiency).

    /Fredrik

  • Hi,

    I am new to BLE programming..

    I am looking for Device Discovery through CC2540 smart kit...

    I have the BLE stack installed from TI..I  have the SIMPLE BLE CENTRAL project..attached the file herewith.

    /**************************************************************************************************
      Filename:       simpleBLECentral.c
      Revised:        $Date: 2011-06-20 11:57:59 -0700 (Mon, 20 Jun 2011) $
      Revision:       $Revision: 28 $
    
      Description:    This file contains the Simple BLE Central sample application 
                      for use with the CC2540 Bluetooth Low Energy Protocol Stack.
    
      Copyright 2010 Texas Instruments Incorporated. All rights reserved.
    
      IMPORTANT: Your use of this Software is limited to those specific rights
      granted under the terms of a software license agreement between the user
      who downloaded the software, his/her employer (which must be your employer)
      and Texas Instruments Incorporated (the "License").  You may not use this
      Software unless you agree to abide by the terms of the License. The License
      limits your use, and you acknowledge, that the Software may not be modified,
      copied or distributed unless embedded on a Texas Instruments microcontroller
      or used solely and exclusively in conjunction with a Texas Instruments radio
      frequency transceiver, which is integrated into your product.  Other than for
      the foregoing purpose, you may not use, reproduce, copy, prepare derivative
      works of, modify, distribute, perform, display or sell this Software and/or
      its documentation for any purpose.
    
      YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
      PROVIDED �AS IS� WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
      INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
      NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
      TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
      NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
      LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
      INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
      OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
      OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
      (INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
    
      Should you have any questions regarding your right to use this Software,
      contact Texas Instruments Incorporated at www.TI.com.
    **************************************************************************************************/
    
    /*********************************************************************
     * INCLUDES
     */
    
    #include "bcomdef.h"
    #include "OSAL.h"
    #include "OSAL_PwrMgr.h"
    #include "OnBoard.h"
    #include "hal_led.h"
    #include "hal_key.h"
    #include "hal_lcd.h"
    #include "gatt.h"
    #include "ll.h"
    #include "hci.h"
    #include "gapgattserver.h"
    #include "gattservapp.h"
    #include "central.h"
    #include "gapbondmgr.h"
    #include "simpleGATTprofile.h"
    #include "simpleBLECentral.h"
    
    /*********************************************************************
     * MACROS
     */
    
    // Length of bd addr as a string
    #define B_ADDR_STR_LEN                        15
    
    /*********************************************************************
     * CONSTANTS
     */
    
    // Maximum number of scan responses
    #define DEFAULT_MAX_SCAN_RES                  8
    
    // Scan duration in ms
    #define DEFAULT_SCAN_DURATION                 4000
    
    // Discovey mode (limited, general, all)
    #define DEFAULT_DISCOVERY_MODE                DEVDISC_MODE_ALL
    
    // TRUE to use active scan
    #define DEFAULT_DISCOVERY_ACTIVE_SCAN         TRUE
    
    // TRUE to use white list during discovery
    #define DEFAULT_DISCOVERY_WHITE_LIST          FALSE
    
    // TRUE to use high scan duty cycle when creating link
    #define DEFAULT_LINK_HIGH_DUTY_CYCLE          FALSE
    
    // TRUE to use white list when creating link
    #define DEFAULT_LINK_WHITE_LIST               FALSE
    
    // Default RSSI polling period in ms
    #define DEFAULT_RSSI_PERIOD                   1000
    
    // Whether to enable automatic parameter update request when a connection is formed
    #define DEFAULT_ENABLE_UPDATE_REQUEST         FALSE
    
    // Minimum connection interval (units of 1.25ms) if automatic parameter update request is enabled
    #define DEFAULT_UPDATE_MIN_CONN_INTERVAL      400
    
    // Maximum connection interval (units of 1.25ms) if automatic parameter update request is enabled
    #define DEFAULT_UPDATE_MAX_CONN_INTERVAL      800
    
    // Slave latency to use if automatic parameter update request is enabled
    #define DEFAULT_UPDATE_SLAVE_LATENCY          0
    
    // Supervision timeout value (units of 10ms) if automatic parameter update request is enabled
    #define DEFAULT_UPDATE_CONN_TIMEOUT           600
    
    // Default passcode
    #define DEFAULT_PASSCODE                      19655
    
    // Default GAP pairing mode
    #define DEFAULT_PAIRING_MODE                  GAPBOND_PAIRING_MODE_WAIT_FOR_REQ
    
    // Default MITM mode (TRUE to require passcode or OOB when pairing)
    #define DEFAULT_MITM_MODE                     FALSE
    
    // Default bonding mode, TRUE to bond
    #define DEFAULT_BONDING_MODE                  TRUE
    
    // Default GAP bonding I/O capabilities
    #define DEFAULT_IO_CAPABILITIES               GAPBOND_IO_CAP_DISPLAY_ONLY
    
    // Default service discovery timer delay in ms
    #define DEFAULT_SVC_DISCOVERY_DELAY           1000
    
    // TRUE to filter discovery results on desired service UUID
    #define DEFAULT_DEV_DISC_BY_SVC_UUID          TRUE
    
    // Application states
    enum
    {
      BLE_STATE_IDLE,
      BLE_STATE_CONNECTING,
      BLE_STATE_CONNECTED,
      BLE_STATE_DISCONNECTING
    };
    
    // Discovery states
    enum
    {
      BLE_DISC_STATE_IDLE,                // Idle
      BLE_DISC_STATE_SVC,                 // Service discovery
      BLE_DISC_STATE_CHAR                 // Characteristic discovery
    };
    
    /*********************************************************************
     * TYPEDEFS
     */
    
    /*********************************************************************
     * GLOBAL VARIABLES
     */
    
    /*********************************************************************
     * EXTERNAL VARIABLES
     */
    
    /*********************************************************************
     * EXTERNAL FUNCTIONS
     */
    
    /*********************************************************************
     * LOCAL VARIABLES
     */
    
    // Task ID for internal task/event processing
    static uint8 simpleBLETaskId;
    
    // GAP GATT Attributes
    static const uint8 simpleBLEDeviceName[GAP_DEVICE_NAME_LEN] = "Simple BLE Central";
    
    // Number of scan results and scan result index
    static uint8 simpleBLEScanRes;
    static uint8 simpleBLEScanIdx;
    
    // Scan result list
    static gapDevRec_t simpleBLEDevList[DEFAULT_MAX_SCAN_RES];
    
    // Scanning state
    static uint8 simpleBLEScanning = FALSE;
    
    // RSSI polling state
    static uint8 simpleBLERssi = FALSE;
    
    // Connection handle of current connection 
    static uint16 simpleBLEConnHandle = GAP_CONNHANDLE_INIT;
    
    // Application state
    static uint8 simpleBLEState = BLE_STATE_IDLE;
    
    // Discovery state
    static uint8 simpleBLEDiscState = BLE_DISC_STATE_IDLE;
    
    // Discovered service start and end handle
    static uint16 simpleBLESvcStartHdl = 0;
    static uint16 simpleBLESvcEndHdl = 0;
    
    // Discovered characteristic handle
    static uint16 simpleBLECharHdl = 0;
    
    // Value to write
    static uint8 simpleBLECharVal = 0;
    
    // Value read/write toggle
    static bool simpleBLEDoWrite = FALSE;
    
    // GATT read/write procedure state
    static bool simpleBLEProcedureInProgress = FALSE;
    
    /*********************************************************************
     * LOCAL FUNCTIONS
     */
    static void simpleBLECentralProcessGATTMsg( gattMsgEvent_t *pMsg );
    static void simpleBLECentralRssiCB( uint16 connHandle, int8  rssi );
    static void simpleBLECentralEventCB( gapCentralRoleEvent_t *pEvent );
    static void simpleBLECentralPasscodeCB( uint8 *deviceAddr, uint16 connectionHandle,
                                            uint8 uiInputs, uint8 uiOutputs );
    static void simpleBLECentralPairStateCB( uint16 connHandle, uint8 state, uint8 status );
    static void simpleBLECentral_HandleKeys( uint8 shift, uint8 keys );
    static void simpleBLECentral_ProcessOSALMsg( osal_event_hdr_t *pMsg );
    static void simpleBLEGATTDiscoveryEvent( gattMsgEvent_t *pMsg );
    static void simpleBLECentralStartDiscovery( void );
    static bool simpleBLEFindSvcUuid( uint16 uuid, uint8 *pData, uint8 dataLen );
    static void simpleBLEAddDeviceInfo( uint8 *pAddr, uint8 addrType );
    char *bdAddr2Str ( uint8 *pAddr );
    
    /*********************************************************************
     * PROFILE CALLBACKS
     */
    
    // GAP Role Callbacks
    static const gapCentralRoleCB_t simpleBLERoleCB =
    {
      simpleBLECentralRssiCB,       // RSSI callback
      simpleBLECentralEventCB       // Event callback
    };
    
    // Bond Manager Callbacks
    static const gapBondCBs_t simpleBLEBondCB =
    {
      simpleBLECentralPasscodeCB,
      simpleBLECentralPairStateCB
    };
    
    /*********************************************************************
     * PUBLIC FUNCTIONS
     */
    
    /*********************************************************************
     * @fn      SimpleBLECentral_Init
     *
     * @brief   Initialization function for the Simple BLE Central App Task.
     *          This is called during initialization and should contain
     *          any application specific initialization (ie. hardware
     *          initialization/setup, table initialization, power up
     *          notification).
     *
     * @param   task_id - the ID assigned by OSAL.  This ID should be
     *                    used to send messages and set timers.
     *
     * @return  none
     */
    void SimpleBLECentral_Init( uint8 task_id )
    {
      simpleBLETaskId = task_id;
    
      // Setup Central Profile
      {
        uint8 scanRes = DEFAULT_MAX_SCAN_RES;
        GAPCentralRole_SetParameter ( GAPCENTRALROLE_MAX_SCAN_RES, sizeof( uint8 ), &scanRes );
      }
      
      // Setup GAP
      GAP_SetParamValue( TGAP_GEN_DISC_SCAN, DEFAULT_SCAN_DURATION );
      GAP_SetParamValue( TGAP_LIM_DISC_SCAN, DEFAULT_SCAN_DURATION );
      GGS_SetParameter( GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN, (uint8 *) simpleBLEDeviceName );
    
      // Setup the GAP Bond Manager
      {
        uint32 passkey = DEFAULT_PASSCODE;
        uint8 pairMode = DEFAULT_PAIRING_MODE;
        uint8 mitm = DEFAULT_MITM_MODE;
        uint8 ioCap = DEFAULT_IO_CAPABILITIES;
        uint8 bonding = DEFAULT_BONDING_MODE;
        GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof( uint32 ), &passkey );
        GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof( uint8 ), &pairMode );
        GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof( uint8 ), &mitm );
        GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof( uint8 ), &ioCap );
        GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof( uint8 ), &bonding );
      }  
    
      // Initialize GATT Client
      VOID GATT_InitClient();
    
      // Register to receive incoming ATT Indications/Notifications
      GATT_RegisterForInd( simpleBLETaskId );
    
      // Initialize GATT attributes
      GGS_AddService( GATT_ALL_SERVICES );         // GAP
      GATTServApp_AddService( GATT_ALL_SERVICES ); // GATT attributes
    
      // Register for all key events - This app will handle all key events
      RegisterForKeys( simpleBLETaskId );
      
      // makes sure LEDs are off
      HalLedSet( (HAL_LED_1 | HAL_LED_2), HAL_LED_MODE_OFF );
      
      // Setup a delayed profile startup
      osal_set_event( simpleBLETaskId, START_DEVICE_EVT );
    }
    
    /*********************************************************************
     * @fn      SimpleBLECentral_ProcessEvent
     *
     * @brief   Simple BLE Central Application Task event processor.  This function
     *          is called to process all events for the task.  Events
     *          include timers, messages and any other user defined events.
     *
     * @param   task_id  - The OSAL assigned task ID.
     * @param   events - events to process.  This is a bit map and can
     *                   contain more than one event.
     *
     * @return  events not processed
     */
    uint16 SimpleBLECentral_ProcessEvent( uint8 task_id, uint16 events )
    {
      
      VOID task_id; // OSAL required parameter that isn't used in this function
      
      if ( events & SYS_EVENT_MSG )
      {
        uint8 *pMsg;
    
        if ( (pMsg = osal_msg_receive( simpleBLETaskId )) != NULL )
        {
          simpleBLECentral_ProcessOSALMsg( (osal_event_hdr_t *)pMsg );
    
          // Release the OSAL message
          VOID osal_msg_deallocate( pMsg );
        }
    
        // return unprocessed events
        return (events ^ SYS_EVENT_MSG);
      }
    
      if ( events & START_DEVICE_EVT )
      {
        // Start the Device
        VOID GAPCentralRole_StartDevice( (gapCentralRoleCB_t *) &simpleBLERoleCB );
    
        // Register with bond manager after starting device
        GAPBondMgr_Register( (gapBondCBs_t *) &simpleBLEBondCB );
    
        return ( events ^ START_DEVICE_EVT );
      }
    
      if ( events & START_DISCOVERY_EVT )
      {
        simpleBLECentralStartDiscovery( );
        
        return ( events ^ START_DISCOVERY_EVT );
      }
      
      // Discard unknown events
      return 0;
    }
    
    /*********************************************************************
     * @fn      simpleBLECentral_ProcessOSALMsg
     *
     * @brief   Process an incoming task message.
     *
     * @param   pMsg - message to process
     *
     * @return  none
     */
    static void simpleBLECentral_ProcessOSALMsg( osal_event_hdr_t *pMsg )
    {
      switch ( pMsg->event )
      {
        case KEY_CHANGE:
          simpleBLECentral_HandleKeys( ((keyChange_t *)pMsg)->state, ((keyChange_t *)pMsg)->keys );
          break;
    
        case GATT_MSG_EVENT:
          simpleBLECentralProcessGATTMsg( (gattMsgEvent_t *) pMsg );
          break;
      }
    }
    
    /*********************************************************************
     * @fn      simpleBLECentral_HandleKeys
     *
     * @brief   Handles all key events for this device.
     *
     * @param   shift - true if in shift/alt.
     * @param   keys - bit field for key events. Valid entries:
     *                 HAL_KEY_SW_2
     *                 HAL_KEY_SW_1
     *
     * @return  none
     */
    uint8 gStatus;
    static void simpleBLECentral_HandleKeys( uint8 shift, uint8 keys )
    {
      (void)shift;  // Intentionally unreferenced parameter
    
      if ( keys & HAL_KEY_UP )
      {
        // Start or stop discovery
        if ( simpleBLEState != BLE_STATE_CONNECTED )
        {
          if ( !simpleBLEScanning )
          {
            simpleBLEScanning = TRUE;
            simpleBLEScanRes = 0;
            
            LCD_WRITE_STRING( "Discovering...", HAL_LCD_LINE_1 );
            LCD_WRITE_STRING( "", HAL_LCD_LINE_2 );
            
            GAPCentralRole_StartDiscovery( DEFAULT_DISCOVERY_MODE,
                                           DEFAULT_DISCOVERY_ACTIVE_SCAN,
                                           DEFAULT_DISCOVERY_WHITE_LIST );      
          }
          else
          {
            GAPCentralRole_CancelDiscovery();
          }
        }
        else if ( simpleBLEState == BLE_STATE_CONNECTED &&
                  simpleBLECharHdl != 0 &&
                  simpleBLEProcedureInProgress == FALSE )
        {
          uint8 status;
          
          // Do a read or write as long as no other read or write is in progress
          if ( simpleBLEDoWrite )
          {
            // Do a write
            attWriteReq_t req;
            
            req.handle = simpleBLECharHdl;
            req.len = 1;
            req.value[0] = simpleBLECharVal;
            req.sig = 0;
            req.cmd = 0;
            status = GATT_WriteCharValue( simpleBLEConnHandle, &req, simpleBLETaskId );         
          }
          else
          {
            // Do a read
            attReadReq_t req;
            
            req.handle = simpleBLECharHdl;
            status = GATT_ReadCharValue( simpleBLEConnHandle, &req, simpleBLETaskId );
          }
          
          if ( status == SUCCESS )
          {
            simpleBLEProcedureInProgress = TRUE;
            simpleBLEDoWrite = !simpleBLEDoWrite;
          }
        }    
      }
    
      if ( keys & HAL_KEY_LEFT )
      {
        // Display discovery results
        if ( !simpleBLEScanning && simpleBLEScanRes > 0 )
        {
            // Increment index of current result (with wraparound)
            simpleBLEScanIdx++;
            if ( simpleBLEScanIdx >= simpleBLEScanRes )
            {
              simpleBLEScanIdx = 0;
            }
            
            LCD_WRITE_STRING_VALUE( "Device", simpleBLEScanIdx + 1,
                                    10, HAL_LCD_LINE_1 );
            LCD_WRITE_STRING( bdAddr2Str( simpleBLEDevList[simpleBLEScanIdx].addr ),
                              HAL_LCD_LINE_2 );
        }
      }
    
      if ( keys & HAL_KEY_RIGHT )
      {
        // Connection update
        if ( simpleBLEState == BLE_STATE_CONNECTED )
        {
          GAPCentralRole_UpdateLink( simpleBLEConnHandle,
                                     DEFAULT_UPDATE_MIN_CONN_INTERVAL,
                                     DEFAULT_UPDATE_MAX_CONN_INTERVAL,
                                     DEFAULT_UPDATE_SLAVE_LATENCY,
                                     DEFAULT_UPDATE_CONN_TIMEOUT );
        }
      }
      
      if ( keys & HAL_KEY_CENTER )
      {
        uint8 addrType;
        uint8 *peerAddr;
        
        // Connect or disconnect
        if ( simpleBLEState == BLE_STATE_IDLE )
        {
          // if there is a scan result
          if ( simpleBLEScanRes > 0 )
          {
            // connect to current device in scan result
            peerAddr = simpleBLEDevList[simpleBLEScanIdx].addr;
            addrType = simpleBLEDevList[simpleBLEScanIdx].addrType;
          
            simpleBLEState = BLE_STATE_CONNECTING;
            
            GAPCentralRole_EstablishLink( DEFAULT_LINK_HIGH_DUTY_CYCLE,
                                          DEFAULT_LINK_WHITE_LIST,
                                          addrType, peerAddr );
      
            LCD_WRITE_STRING( "Connecting", HAL_LCD_LINE_1 );
            LCD_WRITE_STRING( bdAddr2Str( peerAddr ), HAL_LCD_LINE_2 ); 
          }
        }
        else if ( simpleBLEState == BLE_STATE_CONNECTING ||
                  simpleBLEState == BLE_STATE_CONNECTED )
        {
          // disconnect
          simpleBLEState = BLE_STATE_DISCONNECTING;
    
          gStatus = GAPCentralRole_TerminateLink( simpleBLEConnHandle );
          
          LCD_WRITE_STRING( "Disconnecting", HAL_LCD_LINE_1 ); 
        }
      }
      
      if ( keys & HAL_KEY_DOWN )
      {
        // Start or cancel RSSI polling
        if ( simpleBLEState == BLE_STATE_CONNECTED )
        {
          if ( !simpleBLERssi )
          {
            simpleBLERssi = TRUE;
            GAPCentralRole_StartRssi( simpleBLEConnHandle, DEFAULT_RSSI_PERIOD );
          }
          else
          {
            simpleBLERssi = FALSE;
            GAPCentralRole_CancelRssi( simpleBLEConnHandle );
            
            LCD_WRITE_STRING( "RSSI Cancelled", HAL_LCD_LINE_1 );
          }
        }
      }
    }
    
    /*********************************************************************
     * @fn      simpleBLECentralProcessGATTMsg
     *
     * @brief   Process GATT messages
     *
     * @return  none
     */
    static void simpleBLECentralProcessGATTMsg( gattMsgEvent_t *pMsg )
    {
      if ( simpleBLEState != BLE_STATE_CONNECTED )
      {
        // In case a GATT message came after a connection has dropped,
        // ignore the message
        return;
      }
      
      if ( ( pMsg->method == ATT_READ_RSP ) ||
           ( ( pMsg->method == ATT_ERROR_RSP ) &&
             ( pMsg->msg.errorRsp.reqOpcode == ATT_READ_REQ ) ) )
      {
        if ( pMsg->method == ATT_ERROR_RSP )
        {
          uint8 status = pMsg->msg.errorRsp.errCode;
          
          LCD_WRITE_STRING_VALUE( "Read Error", status, 10, HAL_LCD_LINE_1 );
        }
        else
        {
          // After a successful read, display the read value
          uint8 valueRead = pMsg->msg.readRsp.value[0];
    
          LCD_WRITE_STRING_VALUE( "Read rsp:", valueRead, 10, HAL_LCD_LINE_1 );
        }
        
        simpleBLEProcedureInProgress = FALSE;
      }
      else if ( ( pMsg->method == ATT_WRITE_RSP ) ||
           ( ( pMsg->method == ATT_ERROR_RSP ) &&
             ( pMsg->msg.errorRsp.reqOpcode == ATT_WRITE_REQ ) ) )
      {
        
        if ( pMsg->method == ATT_ERROR_RSP == ATT_ERROR_RSP )
        {
          uint8 status = pMsg->msg.errorRsp.errCode;
          
          LCD_WRITE_STRING_VALUE( "Write Error", status, 10, HAL_LCD_LINE_1 );
        }
        else
        {
          // After a succesful write, display the value that was written and increment value
          LCD_WRITE_STRING_VALUE( "Write sent:", simpleBLECharVal++, 10, HAL_LCD_LINE_1 );      
        }
        
        simpleBLEProcedureInProgress = FALSE;    
    
      }
      else if ( simpleBLEDiscState != BLE_DISC_STATE_IDLE )
      {
        simpleBLEGATTDiscoveryEvent( pMsg );
      }
      
    }
    
    /*********************************************************************
     * @fn      simpleBLECentralRssiCB
     *
     * @brief   RSSI callback.
     *
     * @param   connHandle - connection handle
     * @param   rssi - RSSI
     *
     * @return  none
     */
    static void simpleBLECentralRssiCB( uint16 connHandle, int8 rssi )
    {
        LCD_WRITE_STRING_VALUE( "RSSI -dB:", (uint8) (-rssi), 10, HAL_LCD_LINE_1 );
    }
    
    /*********************************************************************
     * @fn      simpleBLECentralEventCB
     *
     * @brief   Central event callback function.
     *
     * @param   pEvent - pointer to event structure
     *
     * @return  none
     */
    static void simpleBLECentralEventCB( gapCentralRoleEvent_t *pEvent )
    {
      switch ( pEvent->gap.opcode )
      {
        case GAP_DEVICE_INIT_DONE_EVENT:  
          {
            LCD_WRITE_STRING( "BLE Central", HAL_LCD_LINE_1 );
            LCD_WRITE_STRING( bdAddr2Str( pEvent->initDone.devAddr ),  HAL_LCD_LINE_2 );
          }
          break;
    
        case GAP_DEVICE_INFO_EVENT:
          {
            // if filtering device discovery results based on service UUID
            if ( DEFAULT_DEV_DISC_BY_SVC_UUID == TRUE )
            {
              if ( simpleBLEFindSvcUuid( SIMPLEPROFILE_SERV_UUID,
                                         pEvent->deviceInfo.pEvtData,
                                         pEvent->deviceInfo.dataLen ) )
              {
                simpleBLEAddDeviceInfo( pEvent->deviceInfo.addr, pEvent->deviceInfo.addrType );
              }
            }
          }
          break;
          
        case GAP_DEVICE_DISCOVERY_EVENT:
          {
            // discovery complete
            simpleBLEScanning = FALSE;
    
            // if not filtering device discovery results based on service UUID
            if ( DEFAULT_DEV_DISC_BY_SVC_UUID == FALSE )
            {
              // Copy results
              simpleBLEScanRes = pEvent->discCmpl.numDevs;
              osal_memcpy( simpleBLEDevList, pEvent->discCmpl.pDevList,
                           (sizeof( gapDevRec_t ) * pEvent->discCmpl.numDevs) );
            }
            
            LCD_WRITE_STRING_VALUE( "Devices Found", simpleBLEScanRes,
                                    10, HAL_LCD_LINE_1 );
            if ( simpleBLEScanRes > 0 )
            {
              LCD_WRITE_STRING( "<- To Select", HAL_LCD_LINE_2 );
            }
    
            // initialize scan index to last device
            simpleBLEScanIdx = simpleBLEScanRes;
    
          }
          break;
    
        case GAP_LINK_ESTABLISHED_EVENT:
          {
            if ( pEvent->gap.hdr.status == SUCCESS )
            {          
              simpleBLEState = BLE_STATE_CONNECTED;
              simpleBLEConnHandle = pEvent->linkCmpl.connectionHandle;
              simpleBLEProcedureInProgress = TRUE;    
    
              // If service discovery not performed initiate service discovery
              if ( simpleBLECharHdl == 0 )
              {
                osal_start_timerEx( simpleBLETaskId, START_DISCOVERY_EVT, DEFAULT_SVC_DISCOVERY_DELAY );
              }
                        
              LCD_WRITE_STRING( "Connected", HAL_LCD_LINE_1 );
              LCD_WRITE_STRING( bdAddr2Str( pEvent->linkCmpl.devAddr ), HAL_LCD_LINE_2 );   
            }
            else
            {
              simpleBLEState = BLE_STATE_IDLE;
              simpleBLEConnHandle = GAP_CONNHANDLE_INIT;
              simpleBLERssi = FALSE;
              simpleBLEDiscState = BLE_DISC_STATE_IDLE;
              
              LCD_WRITE_STRING( "Connect Failed", HAL_LCD_LINE_1 );
              LCD_WRITE_STRING_VALUE( "Reason:", pEvent->gap.hdr.status, 10, HAL_LCD_LINE_2 );
            }
          }
          break;
    
        case GAP_LINK_TERMINATED_EVENT:
          {
            simpleBLEState = BLE_STATE_IDLE;
            simpleBLEConnHandle = GAP_CONNHANDLE_INIT;
            simpleBLERssi = FALSE;
            simpleBLEDiscState = BLE_DISC_STATE_IDLE;
            simpleBLECharHdl = 0;
            simpleBLEProcedureInProgress = FALSE;
              
            LCD_WRITE_STRING( "Disconnected", HAL_LCD_LINE_1 );
            LCD_WRITE_STRING_VALUE( "Reason:", pEvent->linkTerminate.reason,
                                    10, HAL_LCD_LINE_2 );
          }
          break;
    
        case GAP_LINK_PARAM_UPDATE_EVENT:
          {
            LCD_WRITE_STRING( "Param Update", HAL_LCD_LINE_1 );
          }
          break;
          
        default:
          break;
      }
    }
    
    /*********************************************************************
     * @fn      pairStateCB
     *
     * @brief   Pairing state callback.
     *
     * @return  none
     */
    static void simpleBLECentralPairStateCB( uint16 connHandle, uint8 state, uint8 status )
    {
      if ( state == GAPBOND_PAIRING_STATE_STARTED )
      {
        LCD_WRITE_STRING( "Pairing started", HAL_LCD_LINE_1 );
      }
      else if ( state == GAPBOND_PAIRING_STATE_COMPLETE )
      {
        if ( status == SUCCESS )
        {
          LCD_WRITE_STRING( "Pairing success", HAL_LCD_LINE_1 );
        }
        else
        {
          LCD_WRITE_STRING_VALUE( "Pairing fail", status, 10, HAL_LCD_LINE_1 );
        }
      }
      else if ( state == GAPBOND_PAIRING_STATE_BONDED )
      {
        if ( status == SUCCESS )
        {
          LCD_WRITE_STRING( "Bonding success", HAL_LCD_LINE_1 );
        }
      }
    }
    
    /*********************************************************************
     * @fn      simpleBLECentralPasscodeCB
     *
     * @brief   Passcode callback.
     *
     * @return  none
     */
    static void simpleBLECentralPasscodeCB( uint8 *deviceAddr, uint16 connectionHandle,
                                            uint8 uiInputs, uint8 uiOutputs )
    {
    #if (HAL_LCD == TRUE)
    
      uint32  passcode;
      uint8   str[7];
    
      // Create random passcode
      LL_Rand( ((uint8 *) &passcode), sizeof( uint32 ));
      passcode %= 1000000;
      
      // Display passcode to user
      if ( uiOutputs != 0 )
      {
        LCD_WRITE_STRING( "Passcode:",  HAL_LCD_LINE_1 );
        LCD_WRITE_STRING( (char *) _ltoa(passcode, str, 10),  HAL_LCD_LINE_2 );
      }
      
      // Send passcode response
      GAPBondMgr_PasscodeRsp( connectionHandle, SUCCESS, passcode );
    #endif
    }
    
    /*********************************************************************
     * @fn      simpleBLECentralStartDiscovery
     *
     * @brief   Start service discovery.
     *
     * @return  none
     */
    static void simpleBLECentralStartDiscovery( void )
    {
      uint8 uuid[ATT_BT_UUID_SIZE] = { LO_UINT16(SIMPLEPROFILE_SERV_UUID),
                                       HI_UINT16(SIMPLEPROFILE_SERV_UUID) };
      
      // Initialize cached handles
      simpleBLESvcStartHdl = simpleBLESvcEndHdl = simpleBLECharHdl = 0;
    
      simpleBLEDiscState = BLE_DISC_STATE_SVC;
      
      // Discovery simple BLE service
      GATT_DiscPrimaryServiceByUUID( simpleBLEConnHandle,
                                     uuid,
                                     ATT_BT_UUID_SIZE,
                                     simpleBLETaskId );
    }
    
    /*********************************************************************
     * @fn      simpleBLEGATTDiscoveryEvent
     *
     * @brief   Process GATT discovery event
     *
     * @return  none
     */
    static void simpleBLEGATTDiscoveryEvent( gattMsgEvent_t *pMsg )
    {
      attReadByTypeReq_t req;
      
      if ( simpleBLEDiscState == BLE_DISC_STATE_SVC )
      {
        // Service found, store handles
        if ( pMsg->method == ATT_FIND_BY_TYPE_VALUE_RSP &&
             pMsg->msg.findByTypeValueRsp.numInfo > 0 )
        {
          simpleBLESvcStartHdl = pMsg->msg.findByTypeValueRsp.handlesInfo[0].handle;
          simpleBLESvcEndHdl = pMsg->msg.findByTypeValueRsp.handlesInfo[0].grpEndHandle;
        }
        
        // If procedure complete
        if ( ( pMsg->method == ATT_FIND_BY_TYPE_VALUE_RSP  && 
               pMsg->hdr.status == bleProcedureComplete ) ||
             ( pMsg->method == ATT_ERROR_RSP ) )
        {
          if ( simpleBLESvcStartHdl != 0 )
          {
            // Discover characteristic
            simpleBLEDiscState = BLE_DISC_STATE_CHAR;
            
            req.startHandle = simpleBLESvcStartHdl;
            req.endHandle = simpleBLESvcEndHdl;
            req.type.len = ATT_BT_UUID_SIZE;
            req.type.uuid[0] = LO_UINT16(SIMPLEPROFILE_CHAR1_UUID);
            req.type.uuid[1] = HI_UINT16(SIMPLEPROFILE_CHAR1_UUID);
    
            GATT_ReadUsingCharUUID( simpleBLEConnHandle, &req, simpleBLETaskId );
          }
        }
      }
      else if ( simpleBLEDiscState == BLE_DISC_STATE_CHAR )
      {
        // Characteristic found, store handle
        if ( pMsg->method == ATT_READ_BY_TYPE_RSP && 
             pMsg->msg.readByTypeRsp.numPairs > 0 )
        {
          simpleBLECharHdl = BUILD_UINT16( pMsg->msg.readByTypeRsp.dataList[0],
                                           pMsg->msg.readByTypeRsp.dataList[1] );
          
          LCD_WRITE_STRING( "Simple Svc Found", HAL_LCD_LINE_1 );
          simpleBLEProcedureInProgress = FALSE;
        }
        
        simpleBLEDiscState = BLE_DISC_STATE_IDLE;
    
        
      }    
    }
    
    
    /*********************************************************************
     * @fn      simpleBLEFindSvcUuid
     *
     * @brief   Find a given UUID in an advertiser's service UUID list.
     *
     * @return  TRUE if service UUID found
     */
    static bool simpleBLEFindSvcUuid( uint16 uuid, uint8 *pData, uint8 dataLen )
    {
      uint8 adLen;
      uint8 adType;
      uint8 *pEnd;
      
      pEnd = pData + dataLen - 1;
      
      // While end of data not reached
      while ( pData < pEnd )
      {
        // Get length of next AD item
        adLen = *pData++;
        if ( adLen > 0 )
        {
          adType = *pData;
          
          // If AD type is for 16-bit service UUID
          if ( adType == GAP_ADTYPE_16BIT_MORE || adType == GAP_ADTYPE_16BIT_COMPLETE )
          {
            pData++;
            adLen--;
            
            // For each UUID in list
            while ( adLen >= 2 && pData < pEnd )
            {
              // Check for match
              if ( pData[0] == LO_UINT16(uuid) && pData[1] == HI_UINT16(uuid) )
              {
                // Match found
                return TRUE;
              }
              
              // Go to next
              pData += 2;
              adLen -= 2;
            }
            
            // Handle possible erroneous extra byte in UUID list
            if ( adLen == 1 )
            {
              pData++;
            }
          }
          else
          {
            // Go to next item
            pData += adLen;
          }
        }
      }
      
      // Match not found
      return FALSE;
    }
    
    /*********************************************************************
     * @fn      simpleBLEAddDeviceInfo
     *
     * @brief   Add a device to the device discovery result list
     *
     * @return  none
     */
    static void simpleBLEAddDeviceInfo( uint8 *pAddr, uint8 addrType )
    {
      uint8 i;
      
      // If result count not at max
      if ( simpleBLEScanRes < DEFAULT_MAX_SCAN_RES )
      {
        // Check if device is already in scan results
        for ( i = 0; i < simpleBLEScanRes; i++ )
        {
          if ( osal_memcmp( pAddr, simpleBLEDevList[i].addr , B_ADDR_LEN ) )
          {
            return;
          }
        }
        
        // Add addr to scan result list
        osal_memcpy( simpleBLEDevList[simpleBLEScanRes].addr, pAddr, B_ADDR_LEN );
        simpleBLEDevList[simpleBLEScanRes].addrType = addrType;
        
        // Increment scan result count
        simpleBLEScanRes++;
      }
    }
    
    /*********************************************************************
     * @fn      bdAddr2Str
     *
     * @brief   Convert Bluetooth address to string
     *
     * @return  none
     */
    char *bdAddr2Str( uint8 *pAddr )
    {
      uint8       i;
      char        hex[] = "0123456789ABCDEF";
      static char str[B_ADDR_STR_LEN];
      char        *pStr = str;
      
      *pStr++ = '0';
      *pStr++ = 'x';
      
      // Start from end of addr
      pAddr += B_ADDR_LEN;
      
      for ( i = B_ADDR_LEN; i > 0; i-- )
      {
        *pStr++ = hex[*--pAddr >> 4];
        *pStr++ = hex[*pAddr & 0x0F];
      }
      
      *pStr = 0;
      
      return str;
    }
    
    /*********************************************************************
    *********************************************************************/
    

    Could you please tell me the lines that i've to modify in this file to promote the device discovery operation alone..

  • Hi Raghav,

    Line 424: GAPCentralRole_StartDiscovery( DEFAULT_DISCOVERY_MODE, DEFAULT_DISCOVERY_ACTIVE_SCAN, DEFAULT_DISCOVERY_WHITE_LIST );

  • Can you help me in creating a new project for DEVICE Discovery alone...

  • Hi Raghav,

    No, you are on your own on this one :) I recommend going through our documentation and learn how to use our API.

  • Hi,

    OSAL layer---is this a compulsory thing to be included in the programming of CC2540?

  • Hi,

    On each CC254x device, there is a unique IEEE address that can be read using Flash Programmer. OSAL runs the complete stack so you cannot implement you solution without it. This is because all the stack layers tasks/events are executed and prioritized with it. 

    Without OSAL, the solution would be like a lobotomized penguin without a single thought of functional behaviour. You simply need it.

    Best Regards

  • thanks..

    btw I am not creating any app...

    I just need my device to display its MAC-ID when I switch ON the board..So that can be done in HAL itself ryt??