Other Parts Discussed in Thread: CC2540
"Error[e16]: Segment ISTACK (size: 0xc0 align: 0) is too long for segment definition. At least 0xe more bytes needed. The problem occurred while processing the segment placement command "-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#08-_IDATA_END", where at the moment of placement the available memory ranges were "IDATA:4e-ff" Reserved ranges relevant to this placement: IDATA:8-1f VREG IDATA:21-40 VREG IDATA:41-42 XSP IDATA:43-43 DATA_I IDATA:44-4b DATA_Z IDATA:4c-4d IDATA_Z IDATA:4e-ff ISTACK BIT:0-7 BREG BIT:80-97 SFR_AN BIT:a0-af SFR_AN BIT:b8-c7 SFR_AN Error while running Linker " Is there a fix for this problem?