This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 not frequency hopping?



Does this development kit perform frequency hopping when using the TiSmart RF software to monitor the PER/RSSI? As far as I can tell it just sits on a selected channel and transmits. Is there a way to enable frequency hopping with this kit or is it unsupported?

  • Peripheral and broadcaster device advertise on up to 3 dedicated advertising channels. It is only when a connection is established that devices will hop between all other available channels

  • Eng351 said:

    Peripheral and broadcaster device advertise on up to 3 dedicated advertising channels. It is only when a connection is established that devices will hop between all other available channels

    I connected two ble nodes from the kit together using the TISmartRF Software and set it to transmit/receive infinite packets. It did not hop and just sat on the channel the software was set to.