Other Parts Discussed in Thread: CC2540
Hi all,
I need to get advice about connectivity to iOS based device. I tested LightBlue app, which can switch i-device to peripheral mode with advertising. I tried to do connect from CC2540DK configured as Central with connection parameters according to Apple Bluetooth development guidelines. Problem occurred after successfully link establishment - GATT_CharClientCfgUpdated event message is received and after 10 seconds from connection is link terminated with event GAP_LinkTerminated with error code=0x13 (Peer requiered).
Do you know somebody, why is this happening?
I tried to connect i-device from pc with bluez, but it has same affect. I can discover advertising, but about 10 seconds after link establishment to this device is link terminated with same reason=0x13.
I attach log-files, where are captured event messages with iOS. Could someone help me or advice? It's very important for me.
Thank you very much for every help,
Martin Petřík
#hcitool -i hci0 lecc --random 7B:03:8B:F5:4B:CB
< HCI Command: LE Create Connection (0x08|0x000d) plen 25
bdaddr 7B:03:8B:F5:4B:CB type 1
> HCI Event: Command Status (0x0f) plen 4
LE Create Connection (0x08|0x000d) status 0x00 ncmd 1
> HCI Event: LE Meta Event (0x3e) plen 19
LE Connection Complete
status 0x00 handle 64, role master
bdaddr 7B:03:8B:F5:4B:CB (Random)
Connection handle 64
> ACL data: handle 64 flags 0x02 dlen 11
ATT: Read By Group req (0x10)
start 0x0001, end 0xffff
type-uuid 0x2800
> HCI Event: Disconn Complete (0x05) plen 4
status 0x00 handle 64 reason 0x13
Reason: Remote User Terminated Connection
13:14:32.666 -- 13:14:32.666 Packet "GAP_DeviceInit", Opcode 0xfe00 13:14:32.666 Parameters: 13:14:32.666 | profileRole : 8 (GAP_PROFILE_CENTRAL) 13:14:32.666 | maxScanResponses : 3 13:14:32.666 | IRK : "0" 13:14:32.666 | CSRK : "0" 13:14:32.666 | signCounter : 1 13:14:32.666 -- 13:14:32.666 Outgoing Dump: 13:14:32.666 0000: 01 00 fe 26 08 03 00 00 00 00 00 00 00 00 00 00 ...&............ 13:14:32.666 0010: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 13:14:32.666 0020: 00 00 00 00 00 00 01 00 00 00 .......... 13:14:32.670 Incoming Dump: 13:14:32.670 0000: 04 ff 06 7f 06 00 00 fe 00 ......... 13:14:32.695 -- 13:14:32.695 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:32.711 Parameters: 13:14:32.711 | Event Opcode : 0x067f (CommandStatus) 13:14:32.711 | Status : 0x00 (SUCCESS) 13:14:32.711 | opCode : 0xfe00 (GAP_DeviceInit) 13:14:32.711 | dataLen : 0x00 13:14:32.711 -- 13:14:32.712 Incoming Dump: 13:14:32.712 0000: 04 ff 2c 00 06 00 ca e0 09 af 59 90 1b 00 0c 1e ..,.......Y..... 13:14:32.712 0010: 29 96 c9 de 2f 2a 99 89 1e ab 66 71 bd d8 24 eb ).../*....fq..$. 13:14:32.712 0020: 63 65 8d 3d ab 6c 91 8d ee db 25 9a d9 9e 2a ce.=.l....%...* 13:14:32.726 -- 13:14:32.726 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:32.738 Parameters: 13:14:32.738 | Event Opcode : 0x0600 (GAP_DeviceInitDone) 13:14:32.738 | Status : 0x00 (SUCCESS) 13:14:32.738 | devAddr : "90:59:AF:09:E0:CA" 13:14:32.738 | dataPktLen : 0x001b 13:14:32.738 | numDataPkts : 0x0c 13:14:32.738 | IRK : "1E:29:96:C9:DE:2F:2A:99:89:1E:AB:66:71:BD:D8:24" 13:14:32.738 | CSRK : "EB:63:65:8D:3D:AB:6C:91:8D:EE:DB:25:9A:D9:9E:2A" 13:14:32.738 -- 13:14:32.749 -- 13:14:32.749 Packet "GAP_EstablishLinkReq", Opcode 0xfe09 13:14:32.749 Parameters: 13:14:32.749 | highDutyCycle : 0 (Disabled) 13:14:32.749 | whiteList : 0 (Disabled) 13:14:32.749 | addrTypePeer : 0x03 (ADDRTYPE_PRIVATE_RESOLVE) 13:14:32.749 | peerAddr : "40:9B:D2:72:E3:41" 13:14:32.749 -- 13:14:32.749 Outgoing Dump: 13:14:32.749 0000: 01 09 fe 09 00 00 03 41 e3 72 d2 9b 40 .......A.r..@ 13:14:32.756 Incoming Dump: 13:14:32.756 0000: 04 ff 06 7f 06 00 09 fe 00 ......... 13:14:32.768 -- 13:14:32.768 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:32.779 Parameters: 13:14:32.779 | Event Opcode : 0x067f (CommandStatus) 13:14:32.779 | Status : 0x00 (SUCCESS) 13:14:32.779 | opCode : 0xfe09 (GAP_EstablishLinkReq) 13:14:32.779 | dataLen : 0x00 13:14:32.779 -- 13:14:32.876 Incoming Dump: 13:14:32.877 0000: 04 ff 13 05 06 00 03 41 e3 72 d2 9b 40 00 00 50 .......A.r..@..P 13:14:32.877 0010: 00 00 00 d0 07 00 ...... 13:14:32.904 -- 13:14:32.904 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:32.919 Parameters: 13:14:32.919 | Event Opcode : 0x0605 (GAP_LinkEstablished) 13:14:32.919 | Status : 0x00 (SUCCESS) 13:14:32.919 | Device Address Type : 0x03 (ADDRTYPE_PRIVATE_RESOLVE) 13:14:32.919 | Device Address : "40:9B:D2:72:E3:41" 13:14:32.919 | connectionHandle : 0x0000 13:14:32.919 | connInterval : 0x0050 13:14:32.919 | connLatency : 0x0000 13:14:32.919 | connTimeout : 0x07d0 13:14:32.919 | clockAccuracy : 0x00 13:14:32.919 -- 13:14:32.933 -- 13:14:32.933 Packet "GAP_SetParam", Opcode 0xfe30 13:14:32.933 Parameters: 13:14:32.933 | paramID : 21 (TGAP_CONN_EST_INT_MIN) 13:14:32.933 | paramValue : 24 13:14:32.933 -- 13:14:32.933 Outgoing Dump: 13:14:32.933 0000: 01 30 fe 03 15 18 00 .0..... 13:14:32.935 Incoming Dump: 13:14:32.935 0000: 04 ff 06 7f 06 00 30 fe 00 ......0.. 13:14:32.947 -- 13:14:32.947 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:32.959 Parameters: 13:14:32.959 | Event Opcode : 0x067f (CommandStatus) 13:14:32.959 | Status : 0x00 (SUCCESS) 13:14:32.959 | opCode : 0xfe30 (GAP_SetParam) 13:14:32.959 | dataLen : 0x00 13:14:32.959 -- 13:14:32.970 -- 13:14:32.970 Packet "GAP_SetParam", Opcode 0xfe30 13:14:32.970 Parameters: 13:14:32.970 | paramID : 22 (TGAP_CONN_EST_INT_MAX) 13:14:32.970 | paramValue : 312 13:14:32.970 -- 13:14:32.970 Outgoing Dump: 13:14:32.970 0000: 01 30 fe 03 16 38 01 .0...8. 13:14:32.972 Incoming Dump: 13:14:32.972 0000: 04 ff 06 7f 06 00 30 fe 00 ......0.. 13:14:32.984 -- 13:14:32.984 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:32.996 Parameters: 13:14:32.996 | Event Opcode : 0x067f (CommandStatus) 13:14:32.996 | Status : 0x00 (SUCCESS) 13:14:32.996 | opCode : 0xfe30 (GAP_SetParam) 13:14:32.996 | dataLen : 0x00 13:14:32.996 -- 13:14:33.008 -- 13:14:33.008 Packet "GAP_SetParam", Opcode 0xfe30 13:14:33.008 Parameters: 13:14:33.008 | paramID : 26 (TGAP_CONN_EST_LATENCY) 13:14:33.008 | paramValue : 4 13:14:33.008 -- 13:14:33.008 Outgoing Dump: 13:14:33.008 0000: 01 30 fe 03 1a 04 00 .0..... 13:14:33.010 Incoming Dump: 13:14:33.010 0000: 04 ff 06 7f 06 00 30 fe 00 ......0.. 13:14:33.022 -- 13:14:33.022 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:33.033 Parameters: 13:14:33.033 | Event Opcode : 0x067f (CommandStatus) 13:14:33.033 | Status : 0x00 (SUCCESS) 13:14:33.033 | opCode : 0xfe30 (GAP_SetParam) 13:14:33.033 | dataLen : 0x00 13:14:33.033 -- 13:14:33.045 -- 13:14:33.045 Packet "GAP_SetParam", Opcode 0xfe30 13:14:33.045 Parameters: 13:14:33.045 | paramID : 25 (TGAP_CONN_EST_SUPERV_TIMEOUT) 13:14:33.045 | paramValue : 600 13:14:33.045 -- 13:14:33.045 Outgoing Dump: 13:14:33.045 0000: 01 30 fe 03 19 58 02 .0...X. 13:14:33.047 Incoming Dump: 13:14:33.047 0000: 04 ff 06 7f 06 00 30 fe 00 ......0.. 13:14:33.059 -- 13:14:33.059 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:33.071 Parameters: 13:14:33.071 | Event Opcode : 0x067f (CommandStatus) 13:14:33.071 | Status : 0x00 (SUCCESS) 13:14:33.071 | opCode : 0xfe30 (GAP_SetParam) 13:14:33.071 | dataLen : 0x00 13:14:33.071 -- 13:14:33.085 -- 13:14:33.085 *** Script End *** 13:14:33.085 -- 13:14:33.388 Incoming Dump: 13:14:33.388 0000: 04 ff 0a 80 05 00 00 00 04 0f 00 02 00 ............. 13:14:33.413 -- 13:14:33.413 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:33.428 Parameters: 13:14:33.428 | Event Opcode : 0x0580 (GATT_ClientCharCfgUpdated) 13:14:33.428 | Status : 0x00 (SUCCESS) 13:14:33.428 | connectionHandle : 0x0000 13:14:33.428 | pduLen : 0x04 13:14:33.428 | attributeHandle : 0x000f 13:14:33.428 | value : 0x0002 13:14:33.428 -- 13:14:43.085 Incoming Dump: 13:14:43.085 0000: 04 ff 06 06 06 00 00 00 13 ......... 13:14:43.114 -- 13:14:43.114 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff 13:14:43.134 Parameters: 13:14:43.134 | Event Opcode : 0x0606 (GAP_LinkTerminated) 13:14:43.134 | Status : 0x00 (SUCCESS) 13:14:43.134 | connectionHandle : 0x0000 13:14:43.134 | reason : 0x13 (Remote User Terminated Connection) 13:14:43.134 --