Other Parts Discussed in Thread: CC2640
Hy,
to my situation: Since a couple of weeks I have the first 20 samples of a PCB with several sensors and CC2640. They run my firmware quite smoothly, but ever once in a while one of the devices stops: It won't advertise any more and a LED, which I use to signalize special eventy by short blinking, is on constantly.
Thanks to this post I am now able to debug a running target with CCS and XDS100v3. So when I try to connect a "good" device, I can dissamble, set breakpoints, read out memory and register. But when I try to connect a "stopped" target (no advertising, LED on) I see a message
IcePick_C: Error connecting to the target: (Error -275 @ 0x0) The attempt to poll a target device exceeded its timeout limit. The utility or debugger has requested that a target device be repeatedly accessed for a specific data or status value. This has failed because the built-in limit for the maximum number of attempts when polling the JTAG scan-path has been exceeded. (Emulation package 5.1.641.0)
What other possibilities do I have to look into the device? In what state could the processor be? Battery voltage is OK (2,88V), quarz seems to work, as far as I can judge with my limited measurement equipment.
Thank for your help!
Harald