Other Parts Discussed in Thread: ADS1299, CC2650, CC2640, CC2564
Hi all,
I am trying to build a portable wireless EEG system using ADS1299 and I am entangled with wireless module/chip selection.
In my case,I want the output EEG signals of multiple ADS1299s to be transferred to one receiving end wirelessly(star network topology), the throughput is about:
250Hz(sample rate) * 24bits(resolution) * 8(channel) * N(TX-end number)= 48*N kbps
I think the zigbee is too slow for my design and wifi is too power hungry for battery-powered applications, so is bluetooth suitable? I know the max data rate of CC2650 is 1Mbps but what is the max real-world throughput?
If CC2650 is not suitable, could anyone please give me some suggestions on wireless module/chip selection? Thanks!
Regards,
Eric