Hi,
I followed the instructions form http://processors.wiki.ti.com/index.php/CC26xx_LCD to get the Watch dev pack working on the Sensor Tag. I am able to see the test message on the LCD. But the LCD API (devpkLcdText) only works if its used in the SensorTag_init function in the start.
I tried using the API when a key is pressed:
static void SensorTag_callback(PIN_Handle handle, PIN_Id pinId)
{
switch (pinId) {
case Board_KEY_LEFT:
SensorTagKeys_processKeyLeft();
devpkLcdText("Left", 2,0);
break;
case Board_KEY_RIGHT:
SensorTagKeys_processKeyRight();
devpkLcdText("Right", 2,0);
But the application seems to crash when I press the key. Even if I call devpkLcdText on the last line of SensorTag_init it seems to crash.
Can someone please help ?