Hi all,
I am creating a design that uses the CC2640 with the CC2590 gain amplifier. I have been given two different reference schematics for the CC2590:
- the CC2541-CC2590EM schematic here: www.ti.com/.../swrr116
- the CC2590 datasheet:
In the CC2590 datasheet, there are two transmission line inductors,
- 0.87nH on AVDD_PA2 (pin 10), Length=40mil, width=8mil
- 1.54nH on AVDD_LNA (pin 13), length = 100mil, width = 8mil. These were calculated for a 1.6mm thick 4-layer PCB.
In the CC2541-CC2590EM schematic, we have
- 5.1nH chip inductor on AVDD_PA2 (pin 10).
- TLIN inductor of unknown value on AVDD_LNA (pin 13). Measuring the gerber file gives approx 200mils length, and 8mils width. So the length is about twice what is recommended in the datasheet. This is also for a 1.6mm thick 4-layer PCB.
So I have two questions:
1. Are the two circuits equal?
2. If I have a 1mm 4-layer PCB, how would I recalculate the values so the inductances are the same?
Thank you very much for your reply.