This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UniFlash Version: 3.2.0.00023: Error "No repository found at file:/C:/ti/uniflash_3.2/p2tools_repo." when checking for update

Other Parts Discussed in Thread: UNIFLASH, CC3200

Tested with UniFlash Version: 3.2.0.00023:

When checking for updates (via Help -> Check for Updates):

Error message(in a second window)

"No repository found at file:/C:/ti/uniflash_3.2/p2tools_repo."

is displayed behind (first and top window) "No update found".

Note: I have no "p2tools_repo" in "C:/ti/uniflash_3.2"

  • Martin,

    Version: 3.2.0.00023 should not be fetched yet. I guess you downloaded it from the same URL but it has not been announced yet. Once ready, I'll announce it with clear instructions on how to update an existing Uniflash (should be 3.2.0.00019).

    Shlomi

  • Hi Shlomi,

    as same version is now announced (I assume there was no update of uniflash software with same version and same release date) and problem remains the same, here is again my bug report.

    I have this error just after installation of 3.2.0.00023 (just over old version), and selecting "Help" -> "Check for updates".

    Or does it disappear, after a service pack is installed on a real CC3200 the first time?

    Best regards,

    Martin

  • Martin,
    It is reported on the announcement that existing users cannot upgrade due to technical gaps so new Uniflash needs to be installed.

    Sent from my iPhone