I have a CC3200 launchpad and have been using this successfully for weeks, but now I have a problem connecting.
I have all of the jumpers in their default positions...
It seems that I cannot connect to the target for executing/debugging or even flashing using uniflash, unless the "Access Point Mode" jumper is in place (i.e P1-P58).
If I try to run one of the example projects without the P1-P58 jumper in place I get the following error message "Error connecting to the target".
If I try to run the sample example project with the P1-P58 jumper, if downloads and begins to execute then I get the following errors: "Cortex_M4_0: Error " and "Cortex_M4_0: Unable to determine target status after 20 attempts"
I have tried going back and re-running the example projects, but I cant connect any more.
Thanks for your help.
Paul