Hi
I realy need to get thi to work...
i have made a custom board with CC3200 and want to flash it through the FT232RL
but when i start programming with CCS it throws the error:
Cortex_M4_0: GEL Output:
Memory Map Initialization Complete
Cortex_M4_0: Error connecting to the target: Frequency is out of range.
Pin configuration:
SOP0 - 0
SOP1 - 0
SOP2 - 1
FTDI TX - CC GPIO13
FTDI RX - CC GPIO12
Thats pretty much it...
please help!