Other Parts Discussed in Thread: CC2511, CC-DEBUGGER, CC2540
Hi all,
I'm a college student and I have a problem when using a CC2511 transceiver and a oscillator.
I purchased a CC2511 Dongle first and then I designed my own circuit. The schematic is almost the same as the CC2511 Dongle except my PCB does not have a USB interface. I powered my board with a power supply. I checked every pin of the CC2511 chip with a oscilloscope and they are all good. Those pins connected to power all have a 3.3V voltage. I also checked the traces between the pin and the oscillator with a multimeter and the connection is good too. But the oscillator is not working. When I checked the oscillator on the CC2511 Dongle with a oscilloscope, I can see a 48 MHz sine wave. I used the same crystal oscillator as it is recommended in the datasheet of the CC2511 transceiver. But it is not oscillated. What could possibly cause this problem?
Thank you.