Other Parts Discussed in Thread: CC430F6147, CC1101
Hi everybody,
I'm trying to use CC430F6147 evaluation kit to send data at 500 kbaud/sec and I'm facing problems getting high data rates.
In fact, the systems works fine for low data-rates like 10k baud/sec. However when I change the register settings using SmartRF Studio to have 250 or 500 kbaud/sec the same system does not work even if I set the output power to 10 dbm and place the circuits 1 inch from eachother.
As far as I have debugged, at 500 kbaud/sec, packets cannot be recognized. I have a packet counter at the receiver and it shows 5 instead of 120. On the other hand, sometimes the systems just works fine even at 500 kbaud/sec.
Is there anything that I am doing fundamental wrong or it's just how it is?
Thank you very much.