This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Small RF module - CC1200 + CC1190

Other Parts Discussed in Thread: CC1190, CC1200, CC1120

Hi. Currently I' m working on a system that will be something like a watch with RF. That module should communicate with other modules. I want to develop two modules with RF, and I' m interested on CC1200 + CC1190 because of sensibility and tx power.

My questions are:

  • Do you have some Development Kit with CC1200+CC1190? Do you recommend other system or this one (with CC1190) is the best TI RF system for this case (under 1GHZ and with range > 1km)
  • About the antenna, I want to use a small antenna to have a small module and have a quite good range, about 1 km minimum. So it's possible to do it with a chip antenna? Do you have some chip antenna to test? ( 868MHz). 
  • What kind of antenna do you suggest for this system? Chip antenna or other?
  • If I choose CC1200+CC1190, do you have some code that I can use when I build my own system, for example for MSP430?

Thanks in advance, David