Other Parts Discussed in Thread: ENERGIA, CC2640, CC2650, CC1310
Hi,
Is it possible to use MSP432P401R Launchpad onboard XDS110 for CC26xx/CC13xx?
It has JTAG and SWD but it seems that connector J103 provide only SWD signals. Will it work if one uses JTAG lines (TCK_SWCLK; TMS_SWDIO; TDO_SWO; TDI) from differents points on the MSP432P401R Launchpad?
from MSP‑EXP432P401R LaunchPad™ Evaluation Kit User's Guide
2.3.4 Using the XDS110-ET Emulator With a Different Target
The XDS110-ET emulator on the LaunchPad can interface to most ARM derivative devices, not just the on-board MSP432P401R target device. This is not a common use case, but for users who want this functionality, there is a way to enable it. Connector J103 was added to expose all the necessary programming and power signals. J103 is a 50 mil spaced 7-pin header. By default it is not populated, so the user will have to populate a connector or directly solder in wires. When using the XDS110-ET with a different target, the jumpers in the isolation block should be removed, and switch S101 moved to the external debug position. This will disconnect the XDS110-ET from the MSP432P401R target and enable debug of an external device. Because only the SWD signals are exposed, the user needs to set the debugger settings to SWD (without SWO) in the IDE. See the IDE specific MSP432 user's guides for more details on this setting