This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sensortag Debugger DevPack overheating



Hi

When powering a sensortag from the debbuger devpack, I've detected an extreme overheating that almost melted the plastic case of the sensortag. Luckily I reacted before it broke.

As per http://processors.wiki.ti.com/index.php/Debug_DevPack_User_Guide I understand is a possibility to power it this way so, could be this a bug or malfunctioning?

Reading the aforementioned guide, it states that, in order to power the sensortag from the devpack, if the sensortag version is 1.3 and earlier, it must have the coin battery in. My boards are v1.1.3, and I didn't have the coin battery in, can this be the issue? why is this a requirement? does it really power from usb or from the coin battery?

Lot's of questions on this new product ;-)

I have to mention the affected sensortag is running the sample zigbee application for reporting temp and switch, without any tweaking.

By the way, is there any documentation about the accepted inputs for the sensortag bat+/bat- connections? Could I power it directly from a 3.7v LiPo battery?

Thanks a lot, it's a great product!!

Best regards,

Asier.