Other Parts Discussed in Thread: CC2650, CC2538
Select COM port index: 0
Connecting (COM10 @ 230400 baud) ...
100% (480.00ms)
Erasing flash ...
100% (1032.00ms)
Writing flash ...
Warning: CC2650 bootloader will be disabled.
99% Device returned status FLASH_FAIL
100% Device returned status FLASH_FAIL
Error retrying flash download.
- Start address 0x0001FEE4 (page 31).
- Tried to transfer 252 bytes.
- This was transfer 520 in chunk 0.