Other Parts Discussed in Thread: CC1310, SMARTRF06EBK, TEST2
I've tested the new CC1310 with the pre-installed range test firmware on the SmartRF06 board. The test showed that the range was only about 50m at 868Mhz.
Receiver and Transmitter are 1m above ground.
I'd expect to get at least a range of about 500-1000m. This should be possible as the advertisement states it is possible to get a distance of 10km!
What I am missing here?