This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Packet Error Rate Test with CC2650

Other Parts Discussed in Thread: CC2650

Hello , I am student and I am currently working on CC2650 Development Kit for the first time . My purpose is trying a Packet Error Test. I set the Tx and RX in different channels at BLE mode and I have used the 0dB output Power.In certain channels where there is an amount of not received ok packets , when I resend it in the same parameters I don't get the same answer. Is it supposed to be ok? And also i got very confused with noises. When do we consider to have one?

I am just making sure I am on the right track , so I would really appreciate an answer.
thank you in advance