Other Parts Discussed in Thread: CC2531, CC2530
Hi all,
I faced an issue about debugger and the cc2531 dongle, The led is red even if I connect the dongle. The devices are detected by windows so I see them under cebal controlled devices but I can not see them on Flash programmer. I updated the cc debuger's firmware on flash studio, I see the debugger but I can not see the dongle on the connected devices list on flash studio.
I checked the connection and I tried with anothe dongle, the result is same.
I have to connect the dongle because the I need to flash 'cc2531-slip-radio_contikimac' hex file to the dongle since its not listed under the dev path on Contiki.