Other Parts Discussed in Thread: CC1101
This is a question related to the CC1101 sub 1 GHz radio chip. In section 27 of the CC1101 datasheet, it describes the asynchronous serial operation. It explains that the CC1101 modulator samples the level of the asynchronous input 8 times faster than the programmed data rate. Does this 8-time oversampling happen on the TX side or RX side? If it happens on the RX side, does this mean that the RX side must have the knowledge of the TX data rate? If it happens on the TX side, does the RX have to know the TX data rate to be able to demodulate it?