Other Parts Discussed in Thread: TRF7960, MSP430F2370, TRF7960A
Can you tell me what type tags to use and what settings needs to be done in the TRF7960 RHBT to get the maximum response time?
Iread in the blog that HF (13.56MHz) parts can take about 6ms for TX and RX when reading the 64 bit unique ID.
I currently am using the TRF7960EVM (Evaluation Module) that has the MSP430F2370 IRHA MCU.
Will this kit give me the optimum speed I need (minimum of 10mS)?
Can the following issue increase/decrease the response time (how)?
- Type of tag
--ISO standards setting (framing)
-spi/parallel communication with rfid reader and mcu
-clock speed for system and data
-high data rate setting in register (reduces TX power)
-reading a single block only (how does it work
-process in real time MOD(bypass encoder/decoder)
-Voltage supply setting for I/O
- Modulation (ask or ook)
- Demodulation (AM or PM)
- AGC on or off
- Using 12byte FIFO efficiently
- Not use anti-collision/recursive inventory
Can I have a register setting plan so that I can program the RFID receiver via the MCU to maximize and test the read times?
Thanks
Vlad