This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A EVM won't work.

Other Parts Discussed in Thread: TRF7970A

Hi, I want to test the ISO1443A tab with the TRF7970A EVM, but this one won't work...  When I click on the "Set protocol" as described in documentation, the system simply reply with "Read TIMEOUT", but that the few times the EVM is detected...

The driver for COM>USB is installed, and the COM configured on port 2, 115200 bps, 8 data bits, no parity, and 1 stop bit.

For example:


13:46:21.067 --> 01090003040AFF0000
13:46:21.073 --> 010C00030410002101090000
13:46:21.077 COM2
13:46:21.197 <-- TM

13:46:21.201 --> 0109000304F0000000
13:47:03.706 *** Read TIMEOUT ***
13:47:03.710 --> 0109000304F1FF0000
13:47:46.215 *** Read TIMEOUT

Any suggestion?